:CALibrate:SLOT:CRECovery:STATus:DTEMperature?
Query Syntax
:CALibrate:SLOT{1:8}:CRECovery:STATus:DTEMperature?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1. For two-slot modules, the slot number would be 1 or 3. For four-slot modules, like the 86108B, the slot number would be 1.
Description
Queries the change in the N1000A's temperature from the time when the last clock recovery calibration was performed on the indicated slot. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in N1000A temperature exceeds ±5°C. Use the :CALibrate:SLOT:CRECovery command to enable a clock recovery calibration.
Requires FlexDCA revision A.01.70 and above.
Example Returned Status
7.350000000E+00
Example Command
:CALibrate:SLOT2:CRECovery:STATus:DTEMperature?