:CALibrate:SLOT:UTIMebase
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B
Command Syntax
:CALibrate:SLOT{1:8}:UTIMebase {ENABled | DISabled}
Where the required specifier {1:8} identifies an N1093A/B module by slot and must be selected from {1:8}.
Description
Enables or disables an N1093A/B User Timebase Calibration in the specified slot. This calibration takes a few seconds and does not use an external calibration signal. However, the clock trigger jumper cable between the front-panel Clock Trigger Out and In connectors must be installed before running the calibration. If this jumper is not installed, the calibration will pause and prompt you to install the cable.
The N1093A/B is the only DCA-M module that includes a user timebase calibration.
Requires FlexDCA revision A.07.90 and above.
Example Command Sequence
These steps are used for an N1093A/B timebase calibration in slot 5.
:CALibrate:SLOT5:ENABled DISabled :CALibrate:SLOT5:UTIMebase ENABled :CALibrate:SLOT5:STARt :CALibrate:SDONe? # Wait for calibration to complete. :CALibrate:CONTinue # Dismiss calibration dialog. *OPC?