:CALibrate:SLOT:UTIMebase:STATus:DETails?
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B
Query Syntax
:CALibrate:SLOT{1:8}:UTIMebase:STATus:DETails?
Where the required specifier {1:8} identifies an N1093A/B module by slot and must be selected from {1:8}.
Description
Returns a string that provides the date of the last N1093A/B timebase calibration in the indicated slot as well as the elapsed time and the temperature (Celsius) change. Use the :CALibrate:SLOT:UTIMebase:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string:
"Time of last Calibration: 01/08/2014 07:07:12,Elapsed Calibration Time: 8 days,Temperature Change: 1.73 C"
Requires FlexDCA revision A.07.90 and above.
Example Command
:CALibrate:SLOT3:UTIMebase:STATus:DETails?