:CALibrate:SLOT:UTIMebase:STATus?
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B
Query Syntax
:CALibrate:SLOT{1:8}:UTIMebase:STATus?
Where the required specifier {1:8} identifies an N1093A/B module by slot and must be selected from {1:8}.
Query Response
{CALIBRATED | UNCALIBRATED}
Description
Returns the status of the timebase calibration for an N1093A/B module installed in the indicated slot. Use the :CALibrate:SLOT:UTIMebase:DETails, :CALibrate:SLOT:UTIMebase:DTEMperature, and :CALibrate:SLOT:UTIMebase:TIME child commands to return detailed information about the calibration status. Use the :CALibrate:TIMebase:SLOT:STARt command to start a timebase calibration.
Requires FlexDCA revision A.07.90 and above.
Example Command
:CALibrate:SLOT3:UTIMebase:STATus?