:CALibrate:SLOT:UTIMebase:STATus:DTEMperature?
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B
Query Syntax
:CALibrate:SLOT{1:8}:UTIMebase:STATus:DTEMperature?
Where the required specifier {1:8} identifies an N1093A/B module by slot and must be selected from {1:8}.
Description
Returns a string from an N1093A/B DCA-M that provides the change in temperature (Celsius) from the last slot timebase calibration. Use the :CALibrate:SLOT:UTIMebase:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string, which indicates that the temperature has risen 1.73°C:
"1.730000000E+00"
Requires FlexDCA revision A.07.90 and above.
Example Command
:CALibrate:SLOT3:UTIMebase:STATus:DTEMperature?