:CHANnel:FSELect:BANDwidth:MAXimum
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CHANnel{1:8}{A|B|C|D}:FSELect:BANDwidth:MAXimum
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:FSELect:BANDwidth:MAXimum?
Description
If the reference filter for the module can be changed, sets the reference filter to its maximum supported 3 dB bandwidth value. Use the :CHANnel:FILTer command to enable or disable the filter.
- To select or query the minimum supported reference filter 3 dB bandwidth, use the
:CHANnel:FSELect:BANDwidth:MINimumcommand. - To select the reference filter by 3 dB bandwidth or to query the selected value, use the
:CHANnel:FSELect:BANDwidthcommand. - To query the list of available 3 dB bandwidths, use the
:CHANnel:FSELect:BANDwidth:VSET?query. - Although not the preferred method, you can select a reference filter by list order in the Reference Filter field of the channel Setup dialog, use the
:CHANnel:FSELectcommand.
Requires FlexDCA revision A.05.41 and above.
Example Command
:CHANnel2A:FSELect:BANDwidth:MAXimum