:CHANnel:TRANsducer:GAIN
Command Syntax
:CHANnel{1:8}{A|B|C|D}:TRANsducer:GAIN <gain>
Where <gain> is a double.
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:TRANsducer:GAIN?
Description
Enters or queries the gain setting for an external transducer. The measurement units of the offset are the same as the measurement units specified with the :CHANnel:TRANsducer:UNITs command. A query of :CHANnel:TRANsducer:GAIN? always returns a positive value even if negative transducer gain is indicated with the :CHANnel:TRANsducer:INVert command,
To apply the transducer compensation, use the :CHANnel:TRANsducer:STATe command.
Requires FlexDCA revision A.01.80 and above.
Example Command
:CHANnel2A:TRANsducer:GAIN 1.2