:CHANnel:TRANsducer:UNITs
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CHANnel{1:8}{A|B|C|D}:TRANsducer:UNITs {AMPere | VOLT | WATT | UNKNown}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:TRANsducer:UNITs?
Description
Specifies the measurement units for an external transducer's input signal. The AMPere argument is not available for optical channels. To apply the transducer compensation, use the :CHANnel:TRANsducer:STATe command.
Requires FlexDCA revision A.01.80 and above.
Example
:CHANnel2A:TRANsducer:UNITs VOLT