:CRECovery:OUTPut:DMODe
Deprecated command. FlexDCA A.07.90 and above not longer supports the Keysight N4877A Clock/Data Recovery and Demultiplexer.
Command Syntax
:CRECovery{1:8}:OUTPut:DMODe {NORMal | SWAPped}
Where the {1:8} specifier identifies a slot number which is associated with clock recovery module.
Query Syntax
:CRECovery{1:8}:OUTPut:DMODe?
Description
On the N4877A Clock Data Recovery and Demultiplexer extended module, this command swaps the data that is routed to the front-panel DEMUX DATA output ports. This is the output of the demultiplexer. For example, consider if the N4877A input signal is a repeating 10101010 pattern and the output at port OUT1 is 11111… and the output port at OUT2 is 00000…. Using this command with the SWAPped argument would swap the outputs so that the output at OUT1 is 00000… and the output at OUT2 is 11111….
Requires FlexDCA revision A.02.00 and above.