:DISK:EYE:FNAMe:USTandard
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:EYE:FNAMe:USTandard
Description
Resets the file name for the colorgrade-grayscale file from using a custom name to using the standard name in the following form:
cg-gs_<date><autonumber>.<extension>
For example, cg-gs_2020-10-23_1.cgsx. Refer to :DISK:EYE:FNAMe to learn about standard and custom names.
Requires FlexDCA revision A.05.70 and above.