:DISK:EYE:SAVE:SOURce
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:EYE:SAVE:SOURce <source_waveform>
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:DISK:EYE:SAVE:SOURce?
Description
Selects the source for saving to a eye memory (color grade-gray scale memory) file. Use the :DISK:EYE:SAVE parent command to actually save the file.