:DISK:JDATabase:SAVE
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
?
Waveform record:
MV
Instrument:
N1000A
DCA-M
FlexDCA mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:JDATabase:SAVE
Description
In Jitter Mode, saves the jitter database to a file. Use the :DISK:JDATabase:FNAMe command to specify the file name and the :DISK:JDATabase:FFORmat command to specify the file type (.jdx or .csv).
To load a jitter database file into one of FlexDCA's eight eye memories using the :JDMemory:FILE:LOAD and :JDMemory:FILE:NAME commands.
Related Commands
:DISK:JDATabase:FFORmatspecifies the type of file saved.:DISK:JDATabase:FNAMespecifies the saved file's name.:DISK:JDATabase:FNAMe:AUPDateupdates autonumber, if used.:DISK:JDATabase:FNAMe:USTandardresets to the standard file name.