:JDMemory:FILE:NAME
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Command Syntax
:JDMemory{1}:FILE:NAME "filename"
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Query Syntax
:JDMemory{1}:FILE:NAME?
Query Response
"filename"
Description
Enters the name (including path) of a file to be imported into an jitter data memory using the :JDMemory:FILE:LOAD command. If no path is given, the file expected to be in the default \Jitter Data folder.
Requires FlexDCA revision A.05.70 and above.