:DISK:SETup:RECall:HCONfig
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:DISK:SETup:RECall:HCONfig {ON | OFF}
Query Syntax
:DISK:SETup:RECall:HCONfig?
Description
Enables (ON) or disables (OFF) the loading of extended module configurations when a FlexDCA setup file is opened an using the :DISK:SETup:RECall command. Extended module configurations are always saved with a setup file.
Requires FlexDCA revision A.02.00 and above.