:DISK:SIMage:SINClude
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:SIMage:SINClude {CHANnel{1:8}{A|B|C|D} | FUNCtion{1:16} | WMEMory{1:4} | CGMemroy{1:4} | JMEMory1}
Where the {1:8}{A|B|C|D} specifier identifies a specific channel.
Where the {1:16} specifier identifies a specific function.
Where the {1:4} specifier identifies a specific waverform or eye memory.
Query Syntax
:DISK:SIMage:SINClude?
Description
Selects one and only one of any displayed waveforms to be included when saving a screen image using the :DISK:SIMage:SAVE command. By default, all waveforms visible on the display are saved in the screen capture. However, when you select one waveform using this command, all other waveform's will be hidden except for their ground marker (
), which are shown on the screen's right side. Including these markers serves as a reminder that other waveforms were present on the display.