:DISPlay:JITTer:DDJVsbit:NBITs
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.60 and above, use the :DISPlay:JITTer:SGRaph:RANGe command.
Command Syntax
:DISPlay:JITTer:DDJVsbit:NBITs <number_of_bits>
<number_of_bits> is an int.
Query Syntax
:DISPlay:JITTer:DDJVsbit:NBITs?
Description
Sets the number of bits displayed in the DDJ versus Bits graph. Use the :MEASure:JITTer:DDJVsbit command to return the data.
Requires Jitter Mode license.