:DISPlay:JITTer:DDJVsbit:STARt
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.60 and above, use the :DISPlay:JITTer:SGRaph:STARt command.
Command Syntax
:DISPlay:JITTer:DDJVsbit:STARt <start_bit>
<start_bit> is an int.
Query Syntax
:DISPlay:JITTer:DDJVsbit:STARt?
Description
Sets the starting bit displayed in the DDJ versus Bits graph. Use the :MEASure:JITTer:DDJVsbit command to return the data.
Requires Jitter Mode license.