:DISPlay:WINDow:PHASe:TWDouble
Command Syntax
:DISPlay:WINDow:PHASeN:TWDouble {ON | OFF | 1 | 0}
Where N indicates one of 4 possible Phase windows. For example, :PHASe2.
Query Syntax
:DISPlay:WINDow:PHASeN:TWDouble?
Query Response
{1 | 0}
Description
When the Phase waveform content window is displayed, use this command to specify the width of the GrpDelay waveform content window. The window can full width (ON) or half width (OFF). Use the :DISPlay:WINDow:PHASe:LOCation command to align the window with either the left or right edge of the waveform window.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:PHASe2:TWDouble OFF :DISPlay:WINDow:PHASe2:LOCation RSECondary :DISPlay:TSMode HSIZe