:DISPlay:WINDow:MAGNitude:LOCation
Command Syntax
:DISPlay:WINDow:MAGNitudeN:LOCation {PRIMary | LSECondary | RSECondary | FTABs}
Where N indicates one of 4 possible GrpDelay windows. For example, :MAGNitude2.
Query Syntax
:DISPlay:WINDow:MAGNitudeN:LOCation?
Query Response
{PRIM | LSEC | RSEC | FTAB}
Description
Selects the location to display a Freq-Mag (Frequency-Magnitude) waveform content window. Use the arguments listed below to specify the position.
- PRIMary
- The window is placed in the large area normally reserved to display the waveforms.
- LSECondary
- The window is left aligned in a secondary window. Use the
:DISPlay:WINDow:MAGNitude:TWDoublecommand to select whether the window covers the full width or is half the width. If the window is hidden, send the:DISPlay:TSModecommand to expand (show) the window. - RSECondary
- The window is right aligned in a secondary window. Use the
:DISPlay:WINDow:MAGNitude:TWDoublecommand to select whether the window covers the full width or is half the width. If the window is hidden, send the:DISPlay:TSModecommand to expand (show) the window. - FTABs
- The window is undocked (floated) from FlexDCA's window. To re-dock the window, resend the command using the
PRIMary,LSECondary, orRSECondaryarguments.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:MAGNitude2:TWDouble OFF :DISPlay:WINDow:MAGNitude2:LOCation RSECondary :DISPlay:TSMode HSIZe