:DISPlay:WINDow:GDELay{N}:ZSIGnal
Command Syntax
:DISPlay:WINDow:GDELay{N}:ZSIGnal {FUNCtion{1:16} | TRACe{1:128} }
{N} identifies a widow {1:4}.
Query Syntax
:DISPlay:WINDow:GDELay{1:4}:ZSIGnal?
Description
When a GrpDelay (Group Delay) waveform content window is displayed in zoom tiled mode and there are multiple displayed waveforms, selects a waveform to display in the graticule area. The output of the FFT function (FFT command) can be defined as group delay as well as TDR Mode's S-parameters.
Requires FlexDCA revision A.03.00 and above.