:DISPlay:WINDow:MAGNitude:TWDouble
Command Syntax
:DISPlay:WINDow:MAGNitudeN:TWDouble {ON | OFF | 1 | 0}
Where N indicates one of 4 possible Freq-Mag windows. For example, :MAGNitude2.
Query Syntax
:DISPlay:WINDow:MAGNitudeN:TWDouble?
Query Response
{1 | 0}
Description
When the Freq-Mag (Frequency-Magnitude) waveform content window is displayed, use this command to specify the width of the Freq-Mag waveform content window. The window can full width (ON) or half width (OFF). Use the :DISPlay:WINDow:MAGNitude:LOCation command to align the window with either the left or right edge of the waveform window.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:MAGNitude2:TWDouble OFF :DISPlay:WINDow:MAGNitude2:LOCation RSECondary :DISPlay:TSMode HSIZe