:EMEMory:UDEFined:MESial
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Command Syntax
:EMEMory{1:8}:UDEFined:MESial <amplitude>
Where the required specifier {1:8} identifies one of eight eye memories.
Where <amplitude> is an double.
Query Syntax
:EMEMory{1:8}:UDEFined:MESial?
Description
Sets or queries the middle threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :MEASure:THReshold:MESal command.
Use the :MEASure:THReshold:METHod command to specify the use of custom threshold definitions. Use the :MEASure:THReshold:UNITs command to select levels base on absolute amplitude values.
Use the :EMEMory{1:8}:UDEFined:DISTal command to enter a upper threshold level. Use the :EMEMory{1:8}:UDEFined:PROXimal command to enter a lower threshold level.
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs UNITs :MEASure:UTSRc CHANnel1 :EMEMory6:UDEFined:DISTal 125E-3 :EMEMory6:UDEFined:MESial 0E0 :EMEMory6:UDEFined:PROXimal -125E-3