:MEASure:THReshold:METHod
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:THReshold:METHod {P105090 | P205080 | UDEFined}
Query Syntax
:MEASure:THReshold:METHod?
Description
Selects the upper, middle, and lower waveform threshold definitions using the following arguments:
- P105090
- Specifies levels based on 10%, 50%, and 90%.
- P205080
- Specifies levels based on 20%, 50%, and 80%.
- UDEFined
- Selects custom user definitions based on absolute amplitudes. Use the
:MEASure:THReshold:UNITscommand to select levels based on percentages or unit amplitudes. Use the commands listed in the following table to set the actual levels.
| Level | Levels Based On | |
|---|---|---|
| Percentage | Unit Amplitude | |
| Upper Level | :MEASure:THReshold:DISTal | :CHANnel{N}:UDEFined:DISTal
:EMEMory{1:8}:UDEFined:DISTal :WMEMory{1:8}:UDEFined:DISTal :FUNCtion{1:16}:UDEFined:DISTal |
| Middle Level | :MEASure:THReshold:MESial | :CHANnel{N}:UDEFined:MESial
:EMEMory{1:8}:UDEFined:MESial :WMEMory{1:8}:UDEFined:MESial :FUNCtion{1:16}:UDEFined:MESial |
| Lower Level | :MEASure:THReshold:PROXimal | :CHANnel{N}:UDEFined:PROXimal
:EMEMory{1:8}:UDEFined:PROXimal :WMEMory{1:8}:UDEFined:PROXimal :FUNCtion{1:16}:UDEFined:PROXimal |
In Eye/Mask mode, use the :MEASure:THReshold:EREFerence command to establish the reference used when setting the custom threshold-definition levels.
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs UNITs :EMEMory2:UDEFined:DISTal 125E-3 :EMEMory2:UDEFined:MESial 0E0 :EMEMory2:UDEFined:PROXimal -125E-3