:MEASure:THReshold:UNITs

Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:MEASure:THReshold:UNITs  {PERCent | UNITs}

Query Syntax

:MEASure:THReshold:UNITs?

Description

Selects custom threshold definition levels based on percentages (PERCent argument) or absolute amplitudes (UNITs argument). To apply these definitions to measurements, custom threshold definitions must first be selected using the :MEASure:THReshold:METHod command. Depending on the argument, use the commands listed in the following table to set the actual levels.

Commands to Enter Custom Threshold Levels
Level Levels Based On
Percentage Unit Amplitude
Upper Level :MEASure:THReshold:DISTal :CHANnel{N}:UDEFined:DISTal
:EMEMory{1:8}:UDEFined:DISTal
:WMEMory{1:8}:UDEFined:DISTal
:FUNCtion{1:16}:UDEFined:DISTal
Middle Level :MEASure:THReshold:MESial :CHANnel{N}:UDEFined:MESial
:EMEMory{1:8}:UDEFined:MESial
:WMEMory{1:8}:UDEFined:MESial
:FUNCtion{1:16}:UDEFined:MESial
Lower Level :MEASure:THReshold:PROXimal :CHANnel{N}:UDEFined:PROXimal
:EMEMory{1:8}:UDEFined:PROXimal
:WMEMory{1:8}:UDEFined:PROXimal
:FUNCtion{1:16}:UDEFined:PROXimal

Example Command Sequence

:MEASure:THReshold:METHod UDEFined
:MEASure:THReshold:UNITs UNITs
:EMEMory2:UDEFined:DISTal 125E-3
:EMEMory2:UDEFined:MESial 0E0
:EMEMory2:UDEFined:PROXimal -125E-3