:EMODules:SWITch:SADDress
Command Syntax
:EMODules:SWITchN:SADDress <SICL address>
Where N identifies slot number {1:8} which is associated with an optical switch.
Where <SICL address> is a string.
Query Syntax
:EMODules:SWITchN:SADDress?
Description
Specifies the SICL address of an optical switch extended module. To specify a VISA address, use the :SWITch:VADDress command. Use the :SLOT:ADDRess command to select the type of address. Use the :SLOT:CONNect command to actually establish the LAN connection.
Requires FlexDCA revision A.07.00 and above.