:EMODules:SWITch:VADDress
Command Syntax
:EMODules:SWITchN:VADDress <VISA address>
Where N identifies slot number {1:8} which is associated with an optical switch.
Where <VISA address> is a string.
Query Syntax
:EMODules:SWITchN:VADDress?
The query response is: "string"
Description
Specifies the VISA address of an optical switch extended module. To specify a SICL address, use the :SWITch:SADDress command. Use the :SLOT:ADDRess command to select the type of address. Use the :SLOT:CONNect command to actually establish the LAN connection.
Requires FlexDCA revision A.07.00 and above.