:FUNCtion:FOPerator:STATus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Query Syntax
:FUNCtion{1:64}:FOPerator:STATus?
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Description
Queries the status of a function's definition. Some functions require configuration after being created using the :FUNCtion<N>:FOPerator parent command.
- CORR
- The function definition is correct and complete.
- INV
- The function needs configuration to be complets. Use the
:REASonchild command to return a string that indicates the missing information.
Example Command
:FUNCtion2:FOPerator:STATus?