:FUNCtion:FOPerator:STATus:REASon?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Query Syntax
:FUNCtion{1:64}:FOPerator:STATus:REASon?
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Description
Returns a string that indicates the information required to correctly configure a function. For example, the string "Please select a file" would be returned for an incomplete Apply s2p operator.
Example Command
:FUNCtion2:FOPerator:STATus:REASon?