:FUNCtion:XPOSition
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:XPOSition <time>
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Where <time> is an double.
Query Syntax
:FUNCtion{1:64}:XPOSition?
Description
Sets the horizontal time position. The horizontal position is the time delay relative to the trigger event, which is referenced to the display's left edge or center (XREFerence?).
Example Command
:FUNCtion2:XPOSition 6.702E-11