:FUNCtion:XREFerence?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Query Syntax
:FUNCtion{1:64}:XREFerence?
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Description
Queries the horizontal reference which is LEFT or CENTer of the display. The horizontal reference is the reference for specifying a delay, horizontal position (XPOSition?), relative to the trigger event.
Example Command
:FUNCtion2:XREFerence?