:FUNCtion:XSCale
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:XSCale <seconds>
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Where <seconds> is an double.
Query Syntax
:FUNCtion{1:64}:XSCale?
Description
Sets the horizontal time scale in seconds-per-division or symbols, depending on the timebase units setting (:FUNCtion:XUNits). Use the :FUNCtion:XPOSition to set the horizontal position ( time delay relative to the trigger event). Use the :FUNCtion:XLEFt to query the time value at the graticule's left edge and :FUNCtion:XRIGht to squery the time value at the graticule's right edge.
Example Command
:FUNCtion2:XSCale 1.62E-11