:LLINe:HOFFset
Instrument:
N1000A
DCA-M
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
TDR
Command Syntax
:LLINe{1:64}:HOFFset <offset>
Where the {1:64} specifier identifies one of 64 possible limit lines. For example, :LLINe23.
Where <offset> is an double.
Query Syntax
:LLINe{1:64}:HOFFset?
Description
Specifies a horizontal offset in time for the selected Limit Line Test. All limit lines that are defined within the Limit Line Test are shifted by the specified time.
Requires FlexDCA revision A.04.50 and above.
Example
:LLINe2:HOFFset 500E-12