:LLINe:SOURce
Instrument:
N1000A
DCA-M
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
TDR
Command Syntax
:LLINe{1:64}:SOURce <source_waveform>
Where the {1:64} specifier identifies one of 64 possible limit lines. For example, :LLINe23.
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:LLINe{1:64}:SOURce?
Description
Selects the source waveform on with to apply a Limit Line Test.
Requires FlexDCA revision A.04.50 and above.
Command Example
:LLINe8:SOURce CHANnel2A