:LLINe:DISPlay
Instrument:
N1000A
DCA-M
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
TDR
Command Syntax
:LLINe{1:64}:DISPlay {ON | OFF}
Where the {1:64} specifier identifies one of 64 possible limit lines. For example, :LLINe23.
Query Syntax
:LLINe{1:64}:DISPlay?
Description
Loads a Limit Line Test file and displays the test. Up to 64 Limit Line Tests can be simultaneously displayed. To specify the name of the Limit Line Test file to load, use the :LLINe:LOAD:FNAMe command. To select the waveform on which to assign the Limit Line Test, use the :LLINe:SOURce command. To apply horizontal offset to all limit lines that are defined in a displayed Limit Line Test, use the :LLINe:HOFFset command.
After the test has loaded and displayed, use the following commands to return measurement data:
- For the entire Limit Line Test:
:MEASure:LLINe:FPOints?returns the number of displayed failed data points.:MEASure:LLINe:MARGin?returns the pass/fail margin.:MEASure:LLINe:MLOCation?returns the time location of the pass/fail margin.- For a selected limit line in the Limit Line Test:
:MEASure:LLINe:LINE:FPOints?returns the number of displayed failed data points.:MEASure:LLINe:LINE:MARGin?returns the pass/fail margin.:MEASure:LLINe:LINE:MLOCation?returns the time location of the pass/fail margin.
Requires FlexDCA revision A.04.50 and above.
Example
:SYSTem:MODE OSCilloscope :ACQuire:STOP :ACQuire:CDISplay // Load and start limit line test. :LLINe1:LOAD:FNAMe "%USER_DATA_DIR%\Limit Lines\Golden Test.lltx" :LLINe1:SOURce CHANnel1A :LLINe1:DISPlay ON :ACQuire:RUN // Enable data acquisition.