:LTESt:MEASure:MLIMit:FAILures
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:MLIMit{1:16}:FAILures
Where {1:16} identifies one of sixteen limit tests.
Query Syntax
:LTESt:MEASure:MLIMit:FAILures?
Description
Sets the number of failures required to stop the specified measurement limit test. Use the :LTESt:MEASure:MLIMit:STATe command to start the limit test.
Requires FlexDCA revision A.03.00 and above.
Command Example
:LTESt:MEASure:MLIMit2:FALures 5 // Fail test 2 after five failures.