:LTESt:MEASure:MLIMit:STATe
Command Syntax
:LTESt:MEASure:MLIMit{1:16}:STATe {ON | OFF}
Where {1:16} identifies one of sixteen limit tests.
Query Syntax
:LTESt:MEASure:MLIMit:STATe?
Description
Turns the specified measurement limit test, 1 through 16, on or off. Source waveforms include channels, differential channels, and functions. Use the following sibling commands to configure the limit test:
:SOURce:TYPEselects the type of measurement.:SOURce:LOCationselects the actual measurement.:FAILuresdefines the number of failures for stopping a limit test.:FREGionselects when to fail a measurement.:LLIMitdefines the lower limit for failing a measurement.:ULIMitdefines the upper limit for failing a measurement.:UPACtionselects an action if the measurement cannot be performed.
As seen in the example in this topic, the following commands configure the reports of a completed limit test:
:LTESt:MEASure:MLIMit:SIMage:STATe:LTESt:MEASure:MLIMit:SSUMmary:LTESt:MEASure:MLIMit:SWAVeform:CHANnel:STATe:LTESt:MEASure:MLIMit:SWAVeform:DIFF:STATe:LTESt:MEASure:MLIMit:SWAVeform:FUNCtion:STATe
Requires FlexDCA revision A.03.00 and above.
Example Command Sequence
The following example creates three Eye Mode measurement limit tests for the Crossing %, Fall Time, and Rise Time measurements shown in this picture. Notice that the reporting action commands for saving waveform, summary, and a screen capture apply to all active measurement limit tests. The first limit test to complete stops all tests and report actions are taken.
:ACQuire:SINGle // Stop waveform acquisition.// CREATE MEASUREMENT LIMIT TEST 4. :LTESt:MEASure:MLIMit4:SOURce:LOCation 1 // Create test 4 for Crossing % measurement. :LTESt:MEASure:MLIMit4:LLIMit 23E-12 // 23 ps lower limit. :LTESt:MEASure:MLIMit4:ULIMit 24E-12 // 24 ps upper limit. :LTESt:MEASure:MLIMit4:FREGion OUTSide // Fail counted if outside of limit. :LTESt:MEASure:MLIMit4:FAILures 10 // Fail test after 10 failures. :LTESt:MEASure:MLIMit4:UPACtion FAIL // If unable to perform test, fail. :LTESt:MEASure:MLIMit4:STATe ON // Turn Crossing % test on.// CREATE MEASUREMENT LIMIT TEST 5. :LTESt:MEASure:MLIMit5:SOURce:LOCation 2 // Create test 5 for Fall Time measurement. :LTESt:MEASure:MLIMit5:LLIMit 23E-12 // 23 ps lower limit. :LTESt:MEASure:MLIMit5:ULIMit 24E-12 // 24 ps upper limit. :LTESt:MEASure:MLIMit5:FREGion OUTSide // Fail counted if outside of limit. :LTESt:MEASure:MLIMit5:FAILures 10 // Fail test after 10 failures. :LTESt:MEASure:MLIMit5:UPACtion FAIL // If unable to perform test, fail. :LTESt:MEASure:MLIMit5:STATe ON // Turn Fall Time test on.// CREATE MEASUREMENT LIMIT TEST 6. :LTESt:MEASure:MLIMit6:SOURce:LOCation 3 // Create test 6 for Rise Time measurement. :LTESt:MEASure:MLIMit6:LLIMit 23E-12 // 23 ps lower limit. :LTESt:MEASure:MLIMit6:ULIMit 24E-12 // 24 ps upper limit. :LTESt:MEASure:MLIMit6:FREGion OUTSide // Fail counted if outside of limit. :LTESt:MEASure:MLIMit6:FAILures 10 // Fail test after 10 failures. :LTESt:MEASure:MLIMit6:UPACtion FAIL // If unable to perform test, fail. :LTESt:MEASure:MLIMit6:STATe ON // Turn Rise Time test on.// CONFIGURE REPORTING FOR ALL 3 TESTS. :LTESt:MEASure:SWAVeform:CHAN2A:STATe DISK // Save channel 2A data to file. :LTESt:MEASure:SWAVeform:CHAN2A:WMEMory WMEMory3 // Select memory 3. :LTESt:MEASure:SSUMmary:STATe ON // Save summary file. :LTESt:MEASure:SIMage:STATe ON // Save screen image file.// START TESTING. :ACQuire:RUN // Start waveform acquisition. *OPC? // Wait for completion of tests.