:MARKer:X:SOURce:DUT
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MARKer:X{1:4}:SOURce:DUT {DUT{1:16}}
Where the {1:4} specifier identifies one of four markers. For example, :MARKer2.
Query Syntax
:MARKer:X{1:4}:SOURce:DUT?
Description
In TDR mode, use this command along with the :MARKER:X:SOURce:SPARameter command to select a tracking marker's source waveform. This command selects the TDR DUT setup. This command applies only to tracking markers and does not affect manual line markers.
Requires FlexDCA revision A.04.00 and above.