:MARKer:X:STATe

Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:MARKer:X{1:4}:STATe  {OFF | MANual}

Where the {1:4} specifier identifies one of four markers.

Query Syntax

:MARKer:X{1:4}:STATe?

Description

Turns on or off one of four X-axis manual line markers, which can be positioned anywhere along the display's X axis independently of the waveform. Manual line markers have no relationship to any waveform. To turn on a Y-axis manual line marker, use the :MARKer:Y:STATe command.

To turn on a tracking marker, use the :MARKer:Y:STATe command. A tracking marker is designed for single-valued waveforms and can only be placed on sampled waveform points. They cannot be placed between points. This is normally not noticed due to the number of displayed waveform points. If a tracking marker is currently on, the :MARKer:X:STATe? query returns MANual and this marker cannot be turned off using this command. Use the :MARKer:Y:STATe command instead.

MANual
Turns a manual line marker on.
OFF
Turns a manual line marker off.

Example Command Sequence

This example illustrates how to use all of the marker related commands and, as a result, is not presented as a best measurement practice. The example uses a tracking marker, manual line X marker, and manual line Y marker. Because a tracking marker is used, the waveforms must be single-valued. You could also turn on two tracking markers and read the delta values between them.

  //  Configure Manual Line Marker X1
:MARKer:X1:STATe MANual  //  Turn on marker
:MARKer:X1:SOURce CHAN1A  //  Assign marker to Channel 1A waveform
:MARKer:X1:POSition 80E-12  //  Position marker to 80 ps  //  Configure Manual Line Marker Y1
:MARKer:Y1A:STATe MANual  //  Turn on Y manual line marker 1.
:MARKer:Y1A:SOURce CHAN1A  //  Assign marker to Channel 1A waveform
:MARKer:Y1A:POSition 120E-3  //  Position marker to 120 mv
:MARKer:REFerence X1  //  Set markers X1 and Y1 as the reference  //  Configure Tracking Marker Pair 2
:MARKer:Y2A:STATe TRACking  //  Turn on marker
:MARKer:X2:SOURce FUNCtion3  //  Assign marker to FUNCtion3 waveform
:MARKer:X2:POSition 200E-12  //  Position marker on screen

…  //  Prompt tester to position marker on the waveform  //  Return Marker Table Measurements for Tracking Marker 2
:MEASure:MARKer:DX2?  //  Return ΔPosition
:MEASure:MARKer:IDX2?  //  Return inverse of ΔPosition
:MEASure:MARKer:DY2A?  //  Return ΔMagnitude
:MEASure:MARKer:Y2A?  //  Return Y2 Magnitude