:MARKer:X:SOURce:SPARameter
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MARKer:X{1:4}:SOURce:SPARameter <parameter>
Where the {1:4} specifier identifies one of four markers. For example, :MARKer2.
The <parameter> argument is an S-parameter name with an underscore (_) character between the numbers. For example, the argument for an S21 parameter is S2_1.
Query Syntax
:MARKer:X{1:4}:SOURce:SPARameter?
Description
In TDR mode, use this command along with the :MARKER:X:SOURce:DUT command to select a tracking marker's source waveform. This command selects the TDR S-parameter. This command applies only to tracking markers and does not affect manual line markers.
Requires FlexDCA revision A.04.00 and above.