:MEASure:AMPLitude:DEFine:LOCation?

Command:
Deprecated

Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:AMPLitude:DEFine:LOCation:PERCent:LEVel command instead.

Command Syntax

:MEASure:AMPLitude:DEFine:LOCation  <percent>

<percent> is an double.

Query Syntax

:MEASure:AMPLitude:DEFine:LOCation?

Description

Specifies the location within the unit interval at which the noise and interference will be measured. The location is specified as a percentage. 0% corresponds to the left crossing point, 100% corresponds to the right crossing point, and 50% (the default) corresponds to the center of the eye. The specified location must be within the range of 5.0% and 95.0%.

Requires Jitter Mode with additional Advanced Amplitude Analysis/RIN/Q-Factor license .

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.