:MEASure:AMPLitude:DEFine:LOCation:PERCent:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:AMPLitude:DEFine:LOCation:PERCent:LEVel{0|1|2|3} <percent>

<percent> is an double.

Query Syntax

:MEASure:AMPLitude:DEFine:LOCation:PERCent:LEVel?

Description

This command specifies the location within the unit interval at which the noise and interference will be measured on NRZ or PAM4 waveforms. The location is specified as a percentage. A 0% entry corresponds to the left crossing point while a 100% entry corresponds to the right crossing point. A 50% entry (the default) corresponds to the center of the eye. The specified location must be within the range of 5.0% and 95.0%.

For NRZ signals, only the :LEVel0 can be defined and used. For PAM4 signals, four levels can be defined: :LEVel0, :LEVel1, :LEVel2, and :LEVel3.

NRZ Waveform
PAM4 Waveform

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.

Requires FlexDCA revision A.05.60 and above.

This command replaces deprecated command :MEASure:AMPLitude:DEFine:LOCation.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.