:MEASure:AMPLitude:DEFine:RNSValue:ZERO
- Jitter Mode
- :MEASure:AMPLitude:BERFloor?
- :MEASure:AMPLitude:BERFloor:LOCation?
- :MEASure:AMPLitude:BERFloor:SOURce
- :MEASure:AMPLitude:BERFloor:STATus?
- :MEASure:AMPLitude:BERFloor:STATus:REASon?
- :MEASure:AMPLitude:BERLimit?
- :MEASure:AMPLitude:BERLimit:LOCation?
- :MEASure:AMPLitude:BERLimit:SOURce
- :MEASure:AMPLitude:BERLimit:STATus
- :MEASure:AMPLitude:BERLimit:STATus:REASon
- :MEASure:AMPLitude:BIROnes
- :MEASure:AMPLitude:BIROnes:LOCation?
- :MEASure:AMPLitude:BIROnes:SOURce
- :MEASure:AMPLitude:BIROnes:STATus?
- :MEASure:AMPLitude:BIROnes:STATus:REASon?
- :MEASure:AMPLitude:BIRZeros
- :MEASure:AMPLitude:BIRZeros:LOCation?
- :MEASure:AMPLitude:BIRZeros:SOURce
- :MEASure:AMPLitude:BIRZeros:STATus?
- :MEASure:AMPLitude:BIRZeros:STATus:REASon?
- :MEASure:AMPLitude:BUIOnes
- :MEASure:AMPLitude:BUIOnes:LOCation?
- :MEASure:AMPLitude:BUIOnes:SOURce
- :MEASure:AMPLitude:BUIOnes:STATus?
- :MEASure:AMPLitude:BUIOnes:STATus:REASon?
- :MEASure:AMPLitude:BUIZeros?
- :MEASure:AMPLitude:BUIZeros:LOCation?
- :MEASure:AMPLitude:BUIZeros:SOURce
- :MEASure:AMPLitude:BUIZeros:STATus?
- :MEASure:AMPLitude:BUIZeros:STATus:REASon?
- :MEASure:AMPLitude:DEFine:LOCation
- :MEASure:AMPLitude:DEFine:RNCValue:ONE
- :MEASure:AMPLitude:DEFine:RNCValue:ZERO
- :MEASure:AMPLitude:DEFine:RNSValue:ONE
- :MEASure:AMPLitude:DEFine:RNSValue:ZERO
- :MEASure:AMPLitude:DIONes
- :MEASure:AMPLitude:DIONes:LOCation
- :MEASure:AMPLitude:DIONes:SOURce
- :MEASure:AMPLitude:DIONes:STATus
- :MEASure:AMPLitude:DIONes:STATus:REASon
- :MEASure:AMPLitude:DIZeros
- :MEASure:AMPLitude:DIZeros:LOCation
- :MEASure:AMPLitude:DIZeros:SOURce
- :MEASure:AMPLitude:DIZeros:STATus
- :MEASure:AMPLitude:DIZeros:STATus:REASon
- :MEASure:AMPLitude:EOPening:EYE
- :MEASure:AMPLitude:HONE
- :MEASure:AMPLitude:HONE:LOCation
- :MEASure:AMPLitude:HONE:SOURce
- :MEASure:AMPLitude:HONE:STATus
- :MEASure:AMPLitude:HONE:STATus:REASon
- :MEASure:AMPLitude:HZERo
- :MEASure:AMPLitude:HZERo:LOCation
- :MEASure:AMPLitude:HZERo:SOURce
- :MEASure:AMPLitude:HZERo:STATus
- :MEASure:AMPLitude:HZERo:STATus:REASon
- :MEASure:AMPLitude:ISIOnes
- :MEASure:AMPLitude:ISIOnes:LOCation
- :MEASure:AMPLitude:ISIOnes:SOURce
- :MEASure:AMPLitude:ISIOnes:STATus
- :MEASure:AMPLitude:ISIOnes:STATus:REASon
- :MEASure:AMPLitude:ISIVsbit?
- :MEASure:AMPLitude:ISIVsbit:BITS?
- :MEASure:AMPLitude:ISIVsbit:HIGHest?
- :MEASure:AMPLitude:ISIVsbit:LOWest?
- :MEASure:AMPLitude:ISIZeros
- :MEASure:AMPLitude:ISIZeros:LOCation
- :MEASure:AMPLitude:ISIZeros:SOURce
- :MEASure:AMPLitude:ISIZeros:STATus
- :MEASure:AMPLitude:ISIZeros:STATus:REASon
- :MEASure:AMPLitude:LONE
- :MEASure:AMPLitude:LONE:LOCation
- :MEASure:AMPLitude:LONE:SOURce
- :MEASure:AMPLitude:LONE:STATus
- :MEASure:AMPLitude:LONE:STATus:REASon
- :MEASure:AMPLitude:LZERo
- :MEASure:AMPLitude:LZERo:LOCation
- :MEASure:AMPLitude:LZERo:SOURce
- :MEASure:AMPLitude:LZERo:STATus
- :MEASure:AMPLitude:LZERo:STATus:REASon
- :MEASure:AMPLitude:OLEVel
- :MEASure:AMPLitude:OLEVel:LOCation
- :MEASure:AMPLitude:OLEVel:SOURce
- :MEASure:AMPLitude:OLEVel:STATus
- :MEASure:AMPLitude:OLEVel:STATus:REASon
- :MEASure:AMPLitude:PIONes
- :MEASure:AMPLitude:PIONes:LOCation
- :MEASure:AMPLitude:PIONes:SOURce
- :MEASure:AMPLitude:PIONes:STATus
- :MEASure:AMPLitude:PIONes:STATus:REASon
- :MEASure:AMPLitude:PIROnes
- :MEASure:AMPLitude:PIROnes:LOCation
- :MEASure:AMPLitude:PIROnes:SOURce
- :MEASure:AMPLitude:PIROnes:STATus
- :MEASure:AMPLitude:PIROnes:STATus:REASon
- :MEASure:AMPLitude:PIRZeros
- :MEASure:AMPLitude:PIRZeros:LOCation
- :MEASure:AMPLitude:PIRZeros:SOURce
- :MEASure:AMPLitude:PIRZeros:STATus
- :MEASure:AMPLitude:PIRZeros:STATus:REASon
- :MEASure:AMPLitude:PIZeros
- :MEASure:AMPLitude:PIZeros:LOCation
- :MEASure:AMPLitude:PIZeros:SOURce
- :MEASure:AMPLitude:PIZeros:STATus
- :MEASure:AMPLitude:PIZeros:STATus:REASon
- :MEASure:AMPLitude:RNONes
- :MEASure:AMPLitude:RNONes:LOCation
- :MEASure:AMPLitude:RNONes:SOURce
- :MEASure:AMPLitude:RNONes:STATus
- :MEASure:AMPLitude:RNONes:STATus:REASon
- :MEASure:AMPLitude:RNZeros
- :MEASure:AMPLitude:RNZeros:LOCation
- :MEASure:AMPLitude:RNZeros:SOURce
- :MEASure:AMPLitude:RNZeros:STATus
- :MEASure:AMPLitude:RNZeros:STATus:REASon
- :MEASure:AMPLitude:TIONes
- :MEASure:AMPLitude:TIONes:LOCation
- :MEASure:AMPLitude:TIONes:SOURce
- :MEASure:AMPLitude:TIONes:STATus
- :MEASure:AMPLitude:TIONes:STATus:REASon
- :MEASure:AMPLitude:TIZeros
- :MEASure:AMPLitude:TIZeros:SOURce
- :MEASure:AMPLitude:TIZeros:STATus
- :MEASure:AMPLitude:TIZeros:STATus:REASon
- :MEASure:AMPLitude:UNONes
- :MEASure:AMPLitude:UNONes:LOCation
- :MEASure:AMPLitude:UNONes:STATus
- :MEASure:AMPLitude:UNZeros
- :MEASure:AMPLitude:UNZeros:LOCation
- :MEASure:AMPLitude:UNZeros:SOURce
- :MEASure:AMPLitude:UNZeros:STATus
- :MEASure:AMPLitude:UNZeros:STATus:REASon
- :MEASure:AMPLitude:ZLEVel
- :MEASure:AMPLitude:ZLEVel:LOCation
- :MEASure:AMPLitude:ZLEVel:SOURce
- :MEASure:AMPLitude:ZLEVel:STATus
- :MEASure:AMPLitude:ZLEVel:STATus:REASon
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:AMPLitude:DEFine:RNSValue:LEVel command instead.
Command Syntax
:MEASure:AMPLitude:DEFine:RNSValue:ZERO <value>
<value> is an double.
Query Syntax
:MEASure:AMPLitude:DEFine:RNSValue:ZERO?
Description
Enters an RN stabilization value for the zero level. Use the :MEASure:AMPLitude:DEFine:RNSTabliize command to turn RN stabilization on. Manually entering the RN value requires a two-part measurement. First, remove any sources of uncorrelated non-Gaussian, non-periodic noise (for example, cross talk or non-periodic electromagnetic interference). Then, set RN stabilization off and measure the RN. Then, turn RN stabilization on and reapply the sources of uncorrelated non-Gaussian, non-periodic jitter. One use of RN stabilization is to prevent cross talk, from an adjacent channel, appearing as noise. Use the :MEASure:AMPLitude:DEFine:RNSValue:GMRN command to automatically enter the current measured RN value. This RN value will be locked in subsequent jitter measurements.
Requires Jitter Mode with additional Advanced Amplitude Analysis/RIN/Q-Factor license .
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.