:MEASure:AMPLitude:UNONes:SOURce

Command:
Deprecated

Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:AMPLitude:UN:SOURce command instead.

Command Syntax

:MEASure:AMPLitude:UNONes:SOURce  {CHANnel{N} | DIFF{1:8}{A|C} | FUNCtion{1:16} | JMEMory1}

{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.

Query Syntax

:MEASure:AMPLitude:UNONes:SOURce?

Description

Selects the source waveform on which to perform the UNONes measurement.