:MEASure:MARKer:IXDelta:STATus?
Command:
Deprecated
Deprecated command. For FlexDCA revision A.03.00 and above.
Query Syntax
:MEASure:MARKer:IXDelta:STATus?
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the IXDelta measurement. Use the STATus:REASon? child query to determine the reason for a invalid or questionable measurement.