:MEASure:MARKer:IXDelta?
Command:
Deprecated
Deprecated command. For FlexDCA revision A.03.00 and above.
Query Syntax
:MEASure:MARKer:IXDelta?
This command supports the STATus? and STATus:REASon? common child commands.
Description
Queries the reciprocal of the difference in time between any two X-axis markers (1/ΔX): X1 manual marker, X2 manual marker, waveform tracking markers X1/Y1, or waveform tracking markers X2/Y2. The two markers can have different source waveforms. To turn on an X manual marker, use the :MARKer:X<N>:STATe command. To turn on a waveform tracking marker, use the :MARKer:Y<N>:STATe command.
Common Measurement Child Queries
Common measurement queries. :COUNt?, :LOCation?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.
Child Commands
:STATus? queries the measurement status.
:STATus:REASon? query to determine why a measurement failed.
Example Command Sequence
:MARKer:X1:SOURce CHAN2A :MARKer:X2:SOURce CHAN2B // Marker 1 turned on as a manual marker :MARKer:X1:STATe MANual // Marker 2 turned on as a waveform tracking marker :MARKer:Y2:STATe TRAC … … :MEASure:MARKer:IXDelta?