:MEASure:MARKer:XDELta:STATus:REASon?
Command:
Deprecated
Deprecated command. For FlexDCA revision A.03.00 and above.
Query Syntax
:MEASure:MARKer:XDELta:STATus:REASon?
Query Response
Refer to the table "Possible Common :STATus:REASon? Query Responses".
Description
Returns a string that explains the reason for a failed :MARKer:XDELta measurement. If the measurement was successful, a null string is returned. Use the :MARKer:XDELta:STATus? parent query to determine if the measurement has failed.