:MEASure:JITTer:DEFine:PATTern:FILE:NAMe
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:PATTern:FILE:NAMe <file name>
Where <file name> is the name, including path, to a pattern file.
Query Syntax
:MEASure:JITTer:DEFine:PATTern:FILE:NAMe?
Description
In Jitter Mode, enters the name of a BERT pattern file when the :MEASure:JITTer:DEFine:PATTern:MODE command has been used to turn autodetection of the Pattern Symbol Sequence off and specified that a BERT pattern file be used instead. If the name of the pattern file has already been entered (as returned by the query form of this command), you can use the :MEASure:JITTer:DEFine:PATTern:FILE:RELoad command instead.
Requires FlexDCA revision A.07.40 or greater.