:MEASure:JITTer:DEFine:PATTern:FORMat

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:PATTern:FORMat {NRZ | PAM4}

Query Syntax

:MEASure:JITTer:DEFine:PATTern:FORMat?

Description

In Jitter Mode, specifies the format of the input pattern waveform: NRZ or PAM4. You would use this command whenever you have turned off automatic detection of the waveform's Pattern Symbol Sequence with the :MEASure:JITTer:DEFine:PATTern:MODE command.

Requires FlexDCA revision A.07.40 or greater.