:MEASure:JITTer:DEFine:PATTern:TRACking

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DEFine:PATTern:TRACking {OFF}

Query Syntax

:MEASure:JITTer:DEFine:PATTern:TRACking?

Description

In Jitter Mode, turns the tracking of the waveform's Pattern Symbol Sequence on or off. Tracking allows the function to adapt to changes to the signal's pattern.

Requires FlexDCA revision A.07.40 or greater.