:MEASure:JITTer:OJITter:LIST:SELect
Command Syntax
:MEASure:JITTer:OJITter:LIST:SELect <row_index>, <column_index>
<row_index> is an int starting at 1 for the first data row. <column_index> is an int and, although required, it is ignored.
Query Syntax
:MEASure:JITTer:OJITter:LIST:SELect?
Description
In Jitter Mode's Output Jitter panel for 12-Edge Output Jitter PAM4 signals, selects a measurement row in the panel's table. The arguments are two comma-separated integers that represent the table row and column. However, only the row argument is used. The column argument is ignored, but must be supplied. The recommended column index should be 0. Data rows can be specified and selected but not the table heading row. The top measurement is identified as 1,0. For example, in the following figure the highlighted row was selected by sending 5,0. To turn on all 12-Edge Output Jitter PAM4 measurements, use the :MEASure:JITTer:OJITter:STATe command. You cannot remove a table row from the Output Jitter panel as you can with the PAM Eye panel and PAM Level panel.
Requires FlexDCA revision A.06.00 and above.